Hi experts,
Can TS5A21366 switch negative voltages (-200mV to GND) at the NOn and COMn pins? Any concerns?
Thanks and BR,
KF.
TS5A21366DCUR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
KF,
We cannot garuntee the device performance in the electrical characteristics table if the device is being operated outside the recommended operating conditions.
-200mV to GND at the NOn and COMn pins does not violate the absolute maximum ratings -0.5V on NO and COM pins so you will not be at risk of causing permeant damage to the device. The -0.5 V rating is derived from a protection diode from the COM and NO pins to ground which will begin to conduct causing excess leakage current on those pins. Note 4 is saying that this excess current is what can cause the damage to the device and must be limited to <50mA.
Thank you,
Adam