My customer is performing a LTspice simulation of TMUX1072 and used R=18ohm and Con=6.2pF but wonders 6.2pF is the correct value to use:
They are a bit confused about this specifications because the dynamic characteristics would imply that the COM side and the NC,NO side would both have a capacitance of 6.2 pF max.
So we would expect that if the switch is closed the total capacitance is 12.4 pF max but this capacitance is also specified as 6.2 pF.
Could you clarify what the correct channel ON capacitance is?
Thanks
Josef