Hi team,
#1.TS5A2315RSER Device datasheet 6.5 Electrical Characteristics: for 5-V Supply It is mentioned that -40-125℃, VIH=3.1V
so in the condition: VCC=5.0V, VIN1&IN2=3.3V, can it meet the spec of vin_min? If it can be met, vin min is in accordance with 3.1V as stated in datasheet?
#2.A problem about the abnormal switch of TS5A23157HRSER was found on the project. The test data is as follows:
|
normal |
abnormal |
Power-on state pin voltage |
<0.01V |
0.054V |
Pin impedance in power-off state |
infinity |
2MΩ |
do you have some advice on what experiment needed to find the cause?