Other Parts Discussed in Thread: SN74LVC1G3157
Mux Experts,
The power off behavior of this device is causing me considerable consternation.
- In the parametric search this device is listed as having power off protection.
- The datasheet rev history says this feature has been removed from the features section.
- The 0V leakage currents are still in the datasheet
Someone looking for a device to protect a system that has it's power removed from an external signal might think this device is just the ticket for their application and spend considerable resources both financial and otherwise to design it into their application...someone like me. Then after hours of debugging they finally find this forum post which clarifies the behavior of this device:
Adam's last post in this thread is the succinct answer. If power is removed from this device, the internal FET can stay on until VCC = 0. What ends up happening at least in my application is the signal passes through when VCC is removed and then passes through the ESD diodes of devices downstream which in turn holds up the VCC rail enough that the internal FET never turns off. I think its clear that at least some TI'ers are aware of this issue with this device, so why isn't this documented better in the datasheet? It would save engineers using this part valuable time and resources and would lead to a much better customer experience.
Trey