Hello Team,
can you provide typical figure about noise spectrum density of analog switches (e.g. TS5A3166 would be of interest), please?
Especially flicker noise would be of interest.
Thanks and Best Regards,
Hans
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hans,
We do not have this data for this device. I apologize for this - it isn't a spec that we typically characterize on our analog multiplexers.
However the Johnson-Nyquist (thermal noise) can be approximated for the switch. This is because a switch is a pretty simple device and the other errors will come from specs like leakage current.
the noise voltage can be approximated as the following:
where k_b is the Boltzman Constant (1.38 * 10^(-23)) J/K; T is the temperature in Kelvin; R is the Resistance of the switch, and delta f is the bandwidth of interest. If delta f is set as an independent variable you can get an approximated noise figure for the On resistance of interest. There is some complication due to Ron being variable (based on power supplies and input voltage) but using the Ron values in the spec tables can help give a range of possible thermal noise produced.
Flicker noise is a bit trickier to calculate effectively for a switch - so unfortunately we don't have much information on this for this device.
If you have any other questions please let me know!
Best,
Parker Dodson
HI Parker,
I am wondering if there is a way to separate the noise component of switch leakage from the inherent FET physics / schematic driven DC component. Definitely there is a direct relationship between the noise and I,R magnitude that can be leveraged to come up with close approximation.
I understand this is a bit challenging for switches and something to check with the Design team using the precision portfolio (TMUX11xx/TMUX72xx) to model an approximate behavior for the TS5A3166.
Thank you,
Regards,
Sandesh
Hi Hans,
I am sorry for the delay in responses - we are working with our design team to see if this is an okay approximation or if we have a better formula to approximate this. Due to this being a bit more complex issue and with current weather conditions in Dallas our answer time may be delayed, but I will keep you updated - but we may not have more information until next week.
I will keep you updated as more information becomes available.
Best,
Parker Dodson