Hello,
I'm designing a board that will be using 74cb3t16211's as level shifters and pin multiplexers to interface to plug-in modules. In some situations (when a board is not plugged in or where a plug-in board does not use all pins) the nOE of the part will be held high and the pins on one side not connected to anything. Will the weak current pull-up source be sufficient to pull these pins high - it doesn't really matter which state they are pulled into so long as excessive current isn't drawn.
Another 74cb3t16211 will be used to provide configuration pins, where certain pins are pulled low by either jumpers, links or links on the plug in modules. Is it necessary to proved pull up resistors for these inputs?
I'm trying to keep the part count as low as possible
Thanks
D