This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternative to ADG621BRMZ

Other Parts Discussed in Thread: TMUX6212

My customer is looking for an alternative to ADG621BRMZ. Ideally p2p, but this is not a must have. What can we offer?

Thanks

Josef 

  • Hi Josef,

    We do not have any compatible pin-to-pin devices with the ADG621BRMZ. Can you confirm if the application will need dual rail or single rail operation? Are there any other must have requirements for this device (low-RON, voltage range, etc.)?

    Since we have no pin-to-pin solutions, any clarification on the application requirements will help me recommend an appropriate device.

    Thanks!
    Bryan

  • Dear Bryan,

    I sent the request to Josef. It is not important to have a pin-to-pin compatible version. We need 2 channels but could use two single parts as well. R_on can be in the rang up to 20 Ohms, no Problem. We definitivly need dual supply min. +/-5VDC to switch a AC signal at max. 10KHz, +/-3Vp. It ins not important to have a pos. or neg control and we do not need separate controls if you recommend a dual swiches device. Switch on/off timing shall be faster than 100µs.

    BR

    Dieter

  • Hi Dieter,

    Thanks for clearing things up. Given your requirements, I would recommend using the TMUX6212. This is a 4 channel, 1:1 mux, so you would need to GND 2 of the unused inputs. Operating range from +/-4.5V to +/-18V, typical RON of 2ohms, 100ns TON/TOFF, and bandwidth of 56MHz.

    Let me know if this works.

    Thanks!

    Bryan 

  • Dear Bryan,

    TMUX6212 look quite as a good matching on my requirements. Putting two channels in parallel shall be no problem to get an even lower Ron?

    BR

    Dieter

  • Hi Dieter,

    You can certainly do that if you like. Just make sure to tie the correct outputs together as well.

    Thanks!

    Bryan