e2e,
- Can the TMUX6219-Q1 device handle pulses of 300mA for 1.5µs followed by 1mA for 30µs @ 15V DC? I assume, the only limitation is the thermal performance/power losses, right?
- Do you have curves showing the max R_DSon in dependence of Vsup (12V – 23V is of interest)? Or can I do a linear interpolation between the data points of 12V / 32V given in the data sheet?
- Do you have a Spice model?
Thank you,
Adam