• TI thinks resolved

Looking for a better analogue then MC74HC4066

Hello! Help me to find a modern replacement for the 74HC4066 chip.

Options: 4 independent key, the voltage of +5V, the switching frequency is not lower than 30 MHz. The resistance of the keys 4-10 Ohms, or less.

And the most important thing! To the keys inside was controlled antiphase to the control signals into the conclusions of the keys as little as possible!

See in figure? The penetration rate of the control signal on the findings of the key - picovolt