Hi team,
The TS3V713EL datasheet claimed the function of switching between a single VGA source and one of two end points. Is it able to switch 2 sources for 1 end point?
Thanks.
BR,
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mike,
Yes, the TS3V713EL is able to switch 2 sources for 1 end point on some of the signal paths but the TS3V713EL has integrated level sifters on two of the signal paths that are unidirectional. If you would like to have a bi-directional type of switch on all the channels you can use the TS3V712E that does not include the level shifting feature.
Thank you,
Adam