Dear
Please help me review TS3A227E schematic, especially MICP and MIC_PRESENT#,
As below information for your reference, thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear
Please help me review TS3A227E schematic, especially MICP and MIC_PRESENT#,
As below information for your reference, thank you.
Sam,
Power pins: VDD is supplied with 3.3 V and is within the recommended operating conditions.
GND is correctly connected to the thermal pad and the unused GND sense line may also be connected to ground.
Control pins:
I2C SDA/SCL open drain outputs are pulled up to 3.3 V and are within the recommended operating conditions.
INT is an open drain interrupt and I couldn't find where it was going
MIC Present is also and open drain interrupt and it correctly attaches to a GPIO
DET Trigger is correctly connected to a switch in the combo audio jack that will pull the node to ground when a headset is inserted into the Jack
Signal path:
Tip/Ring2/Sleeve correctly connected to the audio jack
Sleeve Sense and Ring2 sense correctly connected to audio jack
MIP correctly connected to the codec.
Also please be aware of this post as well for Apple headsets.
Thank you,
Adam
Dear Adam
Thank you for your reply,
about MIC_PRESENT#, I will connect to "Sense A" pin of codec,
about INT#, I still confirm whether we need this pin,
ALC262 don't have "ground sense pin", so I couldn't connect to "GND_SENSE" of TS3A227E,
last, about C3(in the schematic is C111) that value can vary depending on codec needs,
could I change to 1K ohm?
SCHEMATIC1 _ 0x_AUDIO CODEC_20180412A.pdf
thank you.