I have an application where I would like to switch between DVI and analog VGA signals.
It appears from the product web page and the data sheet that is is possible to pass VGA signals. Real VGA is analog, with a range of perhaps 0 to 2V, depending on termination. The sync signals can be as much as 0-5V. Again, it appears from the data sheet that this should not be a problem, as Vinmax is 5.5V, and this isn't controlled by supply voltage, AFAICT. (I would use 3.3V)
I just want to be sure that I am reading the data sheet correctly and that this is really true.
Thanks!!