Other Parts Discussed in Thread: DP83620, , TS5MP645, TS3DV642
Hello TI,
I am in need of a signal splitting IC which can be used with TI's DP83620 Ethernet Phy.
DP83620 provides only 1 differential output in terms of TX+/- and RX+/- which can be used for both Copper mode and Fiber mode with suitable resistors attached (Reference - DP83620 EVK development Kit).
My application required both Copper and Fiber signal to be designed on the PCB with field configurable option to select either modes. Since the 620 is limited to its number of outputs, can TS3L500 IC be used as where Copper or Fibre mode of Ethernet Phy could be selected by changing its SE pin.Attached an image for reference.
- Since the data sheet does not mentioned 100 Base-FX explicitly, shall it be considered that TS3L500 with work well with my application in fiber mode
- My application has 10/100Base-TX and 100 Base-FX what is the recommended bandwidth of the switching IC
- Since my application would be fulfilled in 4-8 Bit as well so kindly suggest if any.
- Does TI has a simulation tool where I can try these DP83620 with TS3L500 and simiar ICs and verify the signal outputs.
Thank you.