This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS license expired

Prodigy 50 points

Replies: 10

Views: 2138

My licensed CCS studio single user software license expired !  Never understood that it could.

pls advice

 

/Henk  mail :  henk@can-west.nl

  • Guru 130875 points

    Hi Henk,

    what type of license do you have?  I assume a purchased full node locked?  When did you get your license? Could you send a bit more details?  If you send a friend/conversation request you can feel free to send the file itself for a look.

    Best Regards,
    Lisa

  • In reply to Lisa TI:

    Thanks Lisa for your prompt response !

     I will mail you the details and thanks again as I finally found some time to use CCS in a new project.

     

    /Henk 

  • In reply to Henk Hofstra:

    hi Lisa,

    Noticed that I don't have your mail address. 

     

    Product is: CCSSUB
    TMDSCCSSUB-MCUN01-W , which was licenced on 1-21-2010 and expired on 1-21-2011. (just noticed it yesterday, as I never had time to use this product and was not aware that it would expire?)

    note: At the same license date a second CCS product was licensed, but I don't quite understand the difference ?

    TI Part design description: Code Composer Studio IDE - Microcontroller- Node Locked Single User (N01)

    TI Part number : TMDSCCS-MCUN01-v4.0

     

    pls advice and I hope you have a solution for me, as I just now will have to use this product !

     

    thanks,

    /Henk

  • Guru 130875 points

    In reply to Henk Hofstra:

    HI Henk,

    you can simply send me a friend or conversation request with the license file for us to look at.

    What exact message are you getting in CCS?  How do you have CCS configured?  Do I understand you found two license files?  Which is CCS pointing to?

    TI Part number : TMDSCCS-MCUN01-v4.0

    The above part number sounds correct.  This is a full microcontroller node locked license for v4.  Is this what you purchased?  Note if you are trying v5, this is not a v5 license.  So I assume you are using CCSv4?  Is this correct?

    Any further details would help us sort this out.

    Best Regards,
    Lisa

  • In reply to Lisa TI:

    hi Lisa,

     

    This is what is listed in my Regitered software:L

     

    CCSTUDIO
    TMDSCCS-MCUN01-v4.0 

      Code Composer Studio IDE - Microcontroller - Node Locked Single User (N01)  01/21/2010  
     
     Active  9F54-9CC0-A3EE-11DE-B147-D52A-D455-B7B4

    Primary: 00.1F.3A.7D.CE.82
    Not Used  9F4F-1E80-A3EE-11DE-B147-F935-5E22-0DD3

     
    CCSSUB
    TMDSCCSSUB-MCUN01-W   SUBSCRIPTION - Code Composer Studio IDE - Microcontroller - Node Locked Single User (N01)  01/21/2010  
     01/21/2011
    Expired!  Active  9F78-EDA0-A3EE-11DE-B147-EA0B-E79C-9927

    Primary: ANY
    -  9F4F-1E80-A3EE-11DE-B147-F935-5E22-0DD3

    Hope this can solve the issue.

     

    regards,

    /Henk

     

  • Guru 130875 points

    In reply to Henk Hofstra:

    Hi Henk,

    ok, I think it is your subscription, not your license that is expired.

    When you run CCS, can you please confirm that you do no see unlicensed?

    A subscription is what allows major upgrades (if with an active subscription you could migrate to a v5 license for example).


    A CCS license itself never expires.

    Hope this helps.

    Best Regards,
    LIsa

  • In reply to Lisa TI:

    dear Lisa,

     

    As it askes me to register again,cannot use it at all. Problems with the  lic file I suppose as the license cannot expire? Tried to find the lic file but cannot locate it. ( must have lost it after trouble with my computer? )

    As I use my existing license file it is rejected, because it has been used allready.

     

    Hope you can assist me in generating a new liv file, as I must have lost it !

    Thanks again for your help and wait for advice,

     

    /Henk

     

  • Guru 130875 points

    In reply to Henk Hofstra:

    Hi Henk,

    if you lost your .lic file, unfortunately I will have to direct you to the license team at ccs_subscriptions@list.ti.com

    As I said, a node locked license does not expire.  A subscription can and that is what your message shows as expiring. 

    Best Regards,
    Lisa

  • In reply to Lisa TI:

    Thanks Lisa,

    I recieved Henk's email request and hopefully I can help him from here.

    Best Regards,

    Sharon

  • Guru 130875 points

    In reply to Sharon Nigo20:

    Thank you very much Sharon!

    Best Regards,

    Lisa

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.