This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/TIDA-00637: posted source code does not compile with CCS v9.1 - but does work with CCS v6.1.3

Prodigy 70 points

Replies: 2

Views: 88

Part Number: TIDA-00637

Tool/software: Code Composer Studio

The source code posted for this EVSE project here:

http://www.ti.com/tool/TIDC-EVSE-WIFI/

This source code only builds using CCS v6.1.3

It does not build with CCS v9.1

Is it possible to repost this code with the corrections needed to be compatible with the current release of CCS or if someone can provide guidance of necessary changes?

 

  • Guru 166790 points

    Which specific project are you having trouble building? If you are referring to projects in the TIDA-00637 software package, those were designed for CCS 5.2 (as noted in the Readme)  and the version of ARM compiler tools that came with it. You can use CCS 9.1 to build them but would need to set up CCS to discover and use an older version of the compiler tools. Please refer to this page for steps to install a specific version of compiler tools into CCS:
    http://software-dl.ti.com/ccs/esd/documents/ccs_compiler-installation-selection.html

    I would suggest trying a compiler version like 4.4.x or 4.9.x.

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Explore Code Composer Studio documentation and resources using online Resource Explorer
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • Guru 166790 points

    In reply to AartiG:

    Since I haven’t heard back from you, I’m assuming you were able to move past this issue. If not, please feel free to post a reply with an update below (or create a new thread). Thanks!

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Explore Code Composer Studio documentation and resources using online Resource Explorer
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.