This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/TMDSEMU200-U: adapter needed with debugger

Expert 2515 points

Replies: 2

Views: 52

Part Number: TMDSEMU200-U

Tool/software: Code Composer Studio

For the application PCB, I need an adapter like this to use with the XDS200 debugger:

Is this pin to pin compatible? To use this adapter, I need to use one of the adapter boards that came with the debugger.

Thanks,

Priya

  • Guru 147925 points

    Priya,

    The TMDSEMU200-U already comes with a set of pin adapters - check its product page and the photographs.

    http://www.ti.com/tool/TMDSEMU200-U

    The Digi-key adapter you showed is already encompassed by the ARM 10-pin and ARM 20-pin. 

    Hope this helps,

    Rafael


    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    The adapters that came with the debugger were all socket type. I need pin adapter. The connector on the application PCB is not a standard JTAG connector unfortunately. 

    The TM4C EK emulator had a pin connector for standard JTAG and an adapter board used with this is available to connect to the application PCB.

    Priya

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.