This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv51 issues with XGCONF



The XGCONF SYS/BIOS GUI does not work very well in Linux.  I have CCS v5.1.0.07001 installed for both Windows and Linux.  If I open a bios.cfg file with the windows version, I get the SYS/BIOS tab with a GUI screen with the SYS/BIOS - Welcome message at the top.  The System overview tab shows the block diagram and modules can be edited, etc. 

When I open the same bios.cfg file from Linux, sometimes the SYS/BIOS tab is missing altogether.  Sometimes it is present, but the System overview is poorly rendered with fonts outside of the boxes, and the overall layout quite large.  Also in the Linux version, sometimes the outline view does not get filled out.

Is this the proper place to report bugs and issues?