Hi,
Can someone please advise me what the proper way in CCS 5.1 is to create a portable project, i.e. create a project in CCS5.1 on one PC, check the relevant files into source control (such as CVS), check the project out on some other PC also running CCS 5.1, run some batch file to get all the dependencies (if applicable) of the project also from the source control database and automatically perform the necessary configuration steps. After this is done, the user should simply open CCS 5.1 and at this point the project(s) should already be in the workspace and the user would then simply be able to click on build to compile the entire process.
I'm sure there must be an easier way than exporting the project on one PC and then again importing it on the other PC? I came accross a Portable Projects link on the CCS5.1 wiki, but its too cryptic to really get an idea of what the recommended way of doing this is.
Your help would be greatly appreciated!
Regards
Reinier