Hi,
I could not get around this error, my machine is 64-bit Windows 7, CCSv5.2.0 Beta version is installed in C:\ti\...and bios_mcsdk_02_00_05_17 in C:\program Files\Texas Instruments\...
While i am building the PDK, BCP example i am facing the following error
**** Build of configuration Debug for project Bcp_exampleProject ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: C:/Program Files (x86)/Texas Instruments/pdk_C6670_1_0_0_17/packages/ti/drv/bcp/example/bcp.cfg'
'Invoking: XDCtools'
"C:/Program Files (x86)/Texas Instruments/xdctools_3_22_04_46/xs" --xdcpath="C:/Program Files (x86)/Texas Instruments/dsplib_c66x_3_1_0_0/packages;C:/Program Files (x86)/Texas Instruments/edma3_lld_02_11_03_02/packages;C:/ti/grace_1_10_03_30/packages;C:/Program Files (x86)/Texas Instruments/imglib_c66x_3_0_2_1/packages;C:/ti/ipc_1_24_02_27/packages;C:/Program Files (x86)/Texas Instruments/mathlib_c66x_3_0_0_0/packages;C:/Program Files (x86)/Texas Instruments/mcsdk_2_00_05_17/demos;C:/Program Files (x86)/Texas Instruments/pdk_C6670_1_0_0_17/packages;C:/Program Files (x86)/Texas Instruments/pdk_C6678_1_0_0_17/packages;C:/Program Files (x86)/Texas Instruments/ndk_2_20_04_26/packages;C:/ti/bios_6_33_03_34/packages;C:/ti/uia_1_00_03_25/packages;C:/ti/xdais_7_21_01_07/packages;C:/ti/xdais_7_21_01_07/examples;C:/ti/ccsv5/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.C66 -p ti.platforms.evm6670 -r debug -c "C:/ti/ccsv5/tools/compiler/c6000" "C:/Program Files (x86)/Texas Instruments/pdk_C6670_1_0_0_17/packages/ti/drv/bcp/example/bcp.cfg"
The current directory is invalid.
gmake: *** [configPkg/compiler.opt] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Thanks,