My licensed CCS studio single user software license expired ! Never understood that it could.
pls advice
/Henk mail : henk@can-west.nl
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My licensed CCS studio single user software license expired ! Never understood that it could.
pls advice
/Henk mail : henk@can-west.nl
Hi Henk,
what type of license do you have? I assume a purchased full node locked? When did you get your license? Could you send a bit more details? If you send a friend/conversation request you can feel free to send the file itself for a look.
Best Regards,
Lisa
hi Lisa,
Noticed that I don't have your mail address.
Product is: CCSSUB
TMDSCCSSUB-MCUN01-W , which was licenced on 1-21-2010 and expired on 1-21-2011. (just noticed it yesterday, as I never had time to use this product and was not aware that it would expire?)
note: At the same license date a second CCS product was licensed, but I don't quite understand the difference ?
TI Part design description: Code Composer Studio IDE - Microcontroller- Node Locked Single User (N01)
TI Part number : TMDSCCS-MCUN01-v4.0
pls advice and I hope you have a solution for me, as I just now will have to use this product !
thanks,
/Henk
HI Henk,
you can simply send me a friend or conversation request with the license file for us to look at.
What exact message are you getting in CCS? How do you have CCS configured? Do I understand you found two license files? Which is CCS pointing to?
TI Part number : TMDSCCS-MCUN01-v4.0
The above part number sounds correct. This is a full microcontroller node locked license for v4. Is this what you purchased? Note if you are trying v5, this is not a v5 license. So I assume you are using CCSv4? Is this correct?
Any further details would help us sort this out.
Best Regards,
Lisa
hi Lisa,
This is what is listed in my Regitered software:L
CCSTUDIO
TMDSCCS-MCUN01-v4.0
Code Composer Studio IDE - Microcontroller - Node Locked Single User (N01) 01/21/2010
Active 9F54-9CC0-A3EE-11DE-B147-D52A-D455-B7B4
Primary: 00.1F.3A.7D.CE.82
Not Used 9F4F-1E80-A3EE-11DE-B147-F935-5E22-0DD3
CCSSUB
TMDSCCSSUB-MCUN01-W SUBSCRIPTION - Code Composer Studio IDE - Microcontroller - Node Locked Single User (N01) 01/21/2010
01/21/2011
Expired! Active 9F78-EDA0-A3EE-11DE-B147-EA0B-E79C-9927
Primary: ANY
- 9F4F-1E80-A3EE-11DE-B147-F935-5E22-0DD3
Hope this can solve the issue.
regards,
/Henk
Hi Henk,
ok, I think it is your subscription, not your license that is expired.
When you run CCS, can you please confirm that you do no see unlicensed?
A subscription is what allows major upgrades (if with an active subscription you could migrate to a v5 license for example).
A CCS license itself never expires.
Hope this helps.
Best Regards,
LIsa
dear Lisa,
As it askes me to register again,cannot use it at all. Problems with the lic file I suppose as the license cannot expire? Tried to find the lic file but cannot locate it. ( must have lost it after trouble with my computer? )
As I use my existing license file it is rejected, because it has been used allready.
Hope you can assist me in generating a new liv file, as I must have lost it !
Thanks again for your help and wait for advice,
/Henk
Hi Henk,
if you lost your .lic file, unfortunately I will have to direct you to the license team at ccs_subscriptions@list.ti.com
As I said, a node locked license does not expire. A subscription can and that is what your message shows as expiring.
Best Regards,
Lisa
Thanks Lisa,
I recieved Henk's email request and hopefully I can help him from here.
Best Regards,
Sharon