Other Parts Discussed in Thread: TMS570LS3137
Hi there!
I have the following Problem:
I want to program my TMS570, but after writing the 2nd Block i get the following error:
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: Trouble Writing Memory Block at 0x5dc on Page 0 of Length 0x7ff0
CortexR4: Unable to terminate memory download: (Error -1003 @ 0x2BC5) Internal error: Invalid parameter passed to function. Restart the application. If error persists, please report the error. (Emulation package 0.0.0.0)
Target: TMS570LS3137
Programmer: XDS100v2 (BH-100v2-ARM)
CCS: 5.2.1.00018 ( but also tried 5.2.0.00069 with same error)
OS: Ubuntu 12.04.1 LTS
Interestingly I also have a ECC file which loads up without errors.
further the upload works fine with the ECC.out and the prog.out with nowFlash running Windows
thx for the help
Valentin