Other Parts Discussed in Thread: MSP430FR5739, MSP430WARE
I also posted this on MSP430 Forum, but so far no response, but I have following output
error: identifier "class" is undefined
So far I tried everything, including renaming main.c to main.cpp and in
Project => options => Build => MSP430 Compiler => Advanced Options => Language Options => Treat C files as C++ file
My target is MSP430FR5939, and I am using free version of CCS5. Does free version support C++? We are considering switching to this hot new controller, but I cant get started with it, do I need to buy CCS seat or is this CCS bug? Am I doing something wrong. Below is the listing of the class, it chokes on "class"
class CharQueue
{
private:
void start_pp(); // incruments start pointer
void end_pp(); // incruments end pointer
// shoudl be private
unsigned int start; // First character in buffer
unsigned int end; // Next open Character Character in buffer
unsigned char buffer[BUFF_LEN];
public:
CharQueue(); // constructor
int enqueue(unsigned char data[], int data_length); // add string to stack
int enqueue(unsigned char); // add char to stack - overloaded
int buffer_size(); // returns true if stack is not empty
char dequeue_char(); // deque char from stack (DISABLES INTERRUPTS)
};