Other Parts Discussed in Thread: MSP430FR5739
Hi
I am trying to build a simple assembly project for the MSP430FR5739. I have made an simple project where I have two files "testinclude.asm" and "main.asm" but get an [E0300] error when linking. The source is as follows:
testinclude.asm:
****************************************************************
.text
mov.w #1, &ADC10CTL0
****************************************************************
main.asm:
****************************************************************
;-------------------------------------------------------------------------------
; MSP430 Assembler Code Template for use with TI Code Composer Studio
;
;
;-------------------------------------------------------------------------------
.cdecls C,LIST,"msp430.h" ; Include device header file
.include "testinclude.asm"
;-------------------------------------------------------------------------------
.text ; Assemble into program memory
.retain ; Override ELF conditional linking
; and retain current section
.retainrefs ; Additionally retain any sections
; that have references to current
; section
;-------------------------------------------------------------------------------
RESET mov.w #__STACK_END,SP ; Initialize stackpointer
StopWDT mov.w #WDTPW|WDTHOLD,&WDTCTL ; Stop watchdog timer
;-------------------------------------------------------------------------------
; Main loop here
;-------------------------------------------------------------------------------
;-------------------------------------------------------------------------------
; Stack Pointer definition
;-------------------------------------------------------------------------------
.global __STACK_END
.sect .stack
;-------------------------------------------------------------------------------
; Interrupt Vectors
;-------------------------------------------------------------------------------
.sect ".reset" ; MSP430 RESET Vector
.short RESET
****************************************************************
I get the following error when linking:
**** Build of configuration Debug for project TestAssembly ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../main.asm'
'Invoking: MSP430 Compiler'
"C:/ti/ccsv5/tools/compiler/msp430_4.1.4/bin/cl430" -vmspx --abi=eabi -g --include_path="C:/ti/ccsv5/ccs_base/msp430/include" --include_path="C:/ti/ccsv5/tools/compiler/msp430_4.1.4/include" --advice:power=all --define=__MSP430FR5739__ --diag_warning=225 --display_error_number --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --preproc_with_compile --preproc_dependency="main.pp" "../main.asm"
'Finished building: ../main.asm'
' '
'Building file: ../testinclude.asm'
'Invoking: MSP430 Compiler'
"C:/ti/ccsv5/tools/compiler/msp430_4.1.4/bin/cl430" -vmspx --abi=eabi -g --include_path="C:/ti/ccsv5/ccs_base/msp430/include" --include_path="C:/ti/ccsv5/tools/compiler/msp430_4.1.4/include" --advice:power=all --define=__MSP430FR5739__ --diag_warning=225 --display_error_number --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --preproc_with_compile --preproc_dependency="testinclude.pp" "../testinclude.asm"
"../testinclude.asm", ERROR! at EOF: [E0300] The following symbols are undefined:
ADC10CTL0
Errors in Source - Assembler Aborted
1 Assembly Error, No Assembly Warnings
>> Compilation failure
gmake: *** [testinclude.obj] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Why am I getting an error when accessing the defined symbols in msp430fr5739.cmd from my included file and not from main? Remember that main accesses WDTCTL without an error?
Kind regards,
Mads Nielsen