Hello,
I have some troubles evaluating TI example projects since I can't open project configuration files properly.
My installation:
- Windows 7 Professional, Service Pack 1, 64-bit system
- Code Composer Studio version 5.5.0.00077
- AV BIOS SDK version 00 08 00 00
Each example project from the mentioned BIOS package has a configuration file of type "*.cfg", which can be opened with the XGCONF editor. But I have generally a problem to get any other view than the script version of these files. The first tab is always an error report (see attached files), the second one an empty property page, and only the last one, the "cfg script" tab, shows normally a text file.
I encountered this problem already with the previous version 5.4 of CCS, also on another platform (Windows XP on a 32-bit system). Several re-installations and even the update to version 5.5 didn't help out.
Now I wonder how I can solve this issue, Any ideas?