This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS 3.3 windowsXP XDS510 emulator connectivity issue

Prodigy 20 points

Replies: 3

Views: 1423

Guys,

I need some help in resurrecting some legacy program, that uses 2812 on Windows XP as we cannot migrate to new version for field reasons.

My problem is when I am trying to set up CCS with XDS 510 USB emulator, I am failing to connect to the target, when I say Debug-> Connect

The following is the error I get

##################################

Error connecting to the target:
Error 0x80000240/-113
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.

SC_ERR_CTL_HUNG <-113>
The controller's not-ready signal is taking too long.
This often implies one of the following errors:
1. The cable is disconnected near the controller.
2. The cable is disconnected near the target.
3. The JTAG clock has halted.
4. The target power has failed.
5. The controller is in an invalid state and should be reset.


Sequence ID: 0
Error Code: -113
Error Class: 0x80000240
I/O Port = 240

Board Name: F2812 XDS510 Emulator
Cpu Name: CPU_1

Abort:  Close Code Composer Studio.
Retry:  Try to connect to the target again.
Cancel:  Remain disconnected from the target
Diagnostic: Run diagnostic utility.

################################

Any thoughts?? I am using CCs 3.3. When I use SD Config V3.3

  • Guru 301940 points

    Hi Raj,

    What was the output of the SDConfigEx utility?

    Also check the troubleshooting guide from Spectrum Digital's website:

    http://support.spectrumdigital.com/guides/troubleshooting_guide/

    Thanks

    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • In reply to Ki:

    THis is the output of SDConfigEx utility.

     

    * Checking for available printer ports

    ** Checking for available USB ports

      $$ XDS510USB connected on:
      $$ EmuPortAddr=0x510
      $$ EmuSerialNumber=S215500672012522

    ** Using emulation application from directory c:\ccstudio_v3.3pla\drivers
    ** Checking for a valid emulator/eZdsp

      $$ You are connected to:
      $$ EmuProductName=XDS510USB
      $$ EmuPortAddr=0x510
      $$ EmuPortMode=USB
      $$ ProductId=510
      $$ ProductVersion=84


    ** Using emulation application from directory c:\ccstudio_v3.3pla\drivers
    ** Checking for a valid emulator/eZdsp

      $$ You are connected to:
      $$ EmuProductName=XDS510USB
      $$ EmuPortAddr=0x510
      $$ EmuPortMode=USB
      $$ ProductId=510
      $$ ProductVersion=84


    ** Checking emulator/eZdsp scan connection

    ** Emulator Test **

     $$ EmuProductName=XDS510USB

     $$ EmuPortAddr=0x510

     $$ EmuPortMode=USB

     $$ ProductId=510

     $$ ProductVersion=84

     ** Emulator Scan Test

       -- Found JTAG IR length of 38

       -- Found 1 JTAG device(s) in the scan chain

     ________________

    Another issue I see is when I am trying to setup the Connection properties on the Code Composer Studio Setup, in the Connection Properties Tab -> Emulator I/O Port the value is currently at "XDS510 is at port 0x240.

    However in the SCConfigEx

    XDS510USB->Emu->Emulator POrt address is 0x510 by default and this cannot be changed.

    What am I missing?

    -Raj

  • Guru 301940 points

    In reply to Raj Varada1:

    Raj Varada1
    Another issue I see is when I am trying to setup the Connection properties on the Code Composer Studio Setup, in the Connection Properties Tab -> Emulator I/O Port the value is currently at "XDS510 is at port 0x240.

    The setup you are using in CCS is for the TI XDS510 ISA emulator. You need to use the one for the XDS510 USB emulator.

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.