Other Parts Discussed in Thread: TMS320C6657, TMS320DM647
Team,
It seems that some issues have been reported when using multiple emulators (ie having multiple JTAG chains) and multiple instances of CCS 5.5/CCS 6.0 running on the same PC.
I found for example the below CS 5.5 and CCS 6.0 related posts about it:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/292524/1055455.aspx#1055455
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/340152/1191300.aspx#1191300
- Could you please confirm if it is a supported scenario or if we instead encourage to use a single JTAG chain/Single emulator/Single CCS instance to debug multiple processors?
- Looking at the actual the SDSCM00048813 entry it seems that the bug is still present in 6.0 ad not plan to be fixed:
https://cqweb.ext.ti.com/cqweb/#/SDO-Web/SDOWP&format=HTML&version=cqwj
- The actual scenario failing scenario that is seen:
Config: CCS 5.5.0.00077 to debug 2 targets boards with 2 emulators below:
Board DSP EMU
TMDSEVM6657LS TMS320C6657 on board XDS200 mezzanine
custom TMS320DM647 Spectrum Digital XDS510PLUS USB
can start 2 instances of CCS, and start debugging both, with the execution running.
Then pause with a breakpoint one instance. When pressing F6, the other instance of CCS crashes.
No matters which system I'm debugging: if I debug one of these, the other one crashes.
Thanks in advance,
Anthony