hi all,
can i use the memory pragma for dynamic memory allocation?
example:
#pragma DATA_ALIGN(x,16)
int *x;
x=(int*)malloc(variable_size*sizeof(int));
regards
phani tej
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi all,
can i use the memory pragma for dynamic memory allocation?
example:
#pragma DATA_ALIGN(x,16)
int *x;
x=(int*)malloc(variable_size*sizeof(int));
regards
phani tej
If you want to align the address of the dynamically allocated memory, then call memalign() instead of malloc().
[In your example code the DATA_ALIGN will apply to the address of the pointer variable x, rather than the address of dynamically allocated memory]
satya phani tej nittala said:can i use the memory pragma for dynamic memory allocation?
No.
If you build for ARM or C6000, then you call the RTS function memalign. The prototype is ...
void *memalign(size_t _aln, size_t _size);
The first argument is the alignment required, e.g. 16 for 16-byte alignment. The second argument is the number of bytes requested, just like malloc.
Thanks and regards,
-George