This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6000 .cinit format with --rom_mode



Hi all,

I have a question regarding format of .cinit section. I am using C6000 v7.4.8 for a C6748 single core DSP.

The format of the .cinit section in TI-COFF format is specified in TMS320C6000 Optimization Compiler v7.3 section 7.8.5. It consists of a list of cinit records. Further more the following is mentioned:

When you use the --rom_model or --ram_model option, the linker combines the .cinit sections from all the C modules and appends a null word to the end of the composite .cinit section. This terminating record appears as a record with a size field of 0 and marks the end of the initialization tables.

However, if I link with --rom_model I can observe the following:

  • each cinit record is followed by a zero word
  • each cinit record seems to be aligned to a 4 byte address

Note that I am initializing all global variables by myself during startup - therefore I need to parse the .cinit section correctly.

In other words, what is the reason for the holes in .cinit section as observed in the map file:

.cinit     0    00832000    0000141a    
                  00832000    00000d2c     One.obj (.cinit)
                  00832d2c    00000004     --HOLE-- [fill = 00000000]
                  00832d30    0000010a     Two.obj (.cinit)
                  00832e3a    00000006     --HOLE-- [fill = 00000000]
                  00832e40    0000008a     Three.obj (.cinit)
                  00832eca    00000006     --HOLE-- [fill = 00000000]
                  00832ed0    0000007c     Four.obj (.cinit)
                  00832f4c    00000004     --HOLE-- [fill = 00000000]
                  00832f50    0000007c     Five.obj (.cinit)

My compiler options: -k -q -O2 -mv6740 -c

My linker options: -z -q -m"$(PROJECT).map" -x -l"$(CC_BASE)\lib\rts6740.lib"

Thanks in advance

Marc

  • C6000 COFF .cinit records are aligned to 8 bytes. Those holes are just alignment padding for when your data is not exactly a multiple of 8 bytes.
  • Marc Marc said:
    I am initializing all global variables by myself during startup - therefore I need to parse the .cinit section correctly.

    Code that parses the .cinit tables is supplied with the compiler RTS source code.  Look for the file autoinit.c in a directory similar to ...

    C:\ti\ccsv6\tools\compiler\c6000_7.4.14\lib\src

    Thanks and regards,

    -George