This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C64XP_0: Error connecting to the target: Connect to PRSC failed, -6305 in linux ( DM6446 EVM Board)

  • Version of the host OS:  Ubuntu 12.04 1GB 32-bit
  • CCS Version: 5.4.0.00091
  • DM6446 EVM Board,Emulator : Spectrum Digital XDS510 USB

I am trying to debug message application provided by DSPLINK in DM6446 EVM board

I am running ./messagegpp message.out  100 in linux and

         When I try to debug  using CCS  I get  the foolowing error "C64XP_0: Error connecting to the target: Connect to PRSC failed, -6305 "

Any help will be appreciated.

Regards

Sridevi M