Other Parts Discussed in Thread: TM4C123GH6PM, CC2640
I am designing a circuit in which I am going to connect ARM 20 Pin JTAG to tm4c123gh6pm using following pins.
As per explained on page processors.wiki.ti.com/.../XDS_Target_Connection_Guide
| JTAG connector | ARM 20-Pin5 | |
| Pin number | ||
| 1 | VTRef | |
| 2 | VSupply | |
| 3 | nTRST | |
| 4 | GND | |
| 5 | TDI | |
| 6 | GND | |
| 7 | SWDIO / TMS | |
| 8 | GND | |
| 9 | SWDCLK / TCK | |
| 10 | GND | |
| 11 | RTCK | |
| 12 | GND | |
| 13 | SWO / TDO | |
| 14 | GND | |
| 15 | nRESET | |
| 16 | GND | |
| 17 | NC / DBGRQ | |
| 18 | GND | |
| 19 | NC / DBGACK | |
| 20 | GND | |
These connections will be connected to four standard pins: TCK (52), TMS (51), TDI (50), and TDO (49)
Is this connection correct for TMDSEMU100v2U-ARM 20 pin JTAG to Tiva C series MicroController. ?
Much more confusion on page XDS_Target_Connection_Guide