Dear All,
We are using DSP TMS320C6748EZWTD4E in our custom board same as EVMC6748.
We are using CCS-5.4 with JTAG XDS100v2 USB emulator.
We have set boot mode pins BOOT[7:0] = 0001 1110 (Emulation Debug)
Also, the JTAG scan test is passed successfully.
When we try to connect with the board, we are getting the following error message :-
"C674X_0: Error connecting to the target: Connect to PRSC failed"
We have already tested reset circuit and it is working properly.
Kindly help us to get rid of this problem asap.
Thanks & Regards
Srikanta