Using CCS 6.1.3.00033 created a new project for the Cortex-A15 in a 66AK2H14 using the GNU v4.9.3 compiler. After creating the project there were no startup file or linker script added by CCS so:
- Copied the ccsv6\ccs_base\arm\include\startup_ARMCA15.S file into the project
- Copied the ccsv6\ccs_base\arm\include\66AK2Gxx.lds file into the project, and changed to store the program in DDR0 (the 66AK2Gxx.lds linker script was the closest example for the target device)
In the CCS project properties -float-abi was set to "hard" and -mfpu was set to "vfp4" to enable hardware floating point, which then causes the startup_ARMCA15.S file to enable NEON extensions and the VFP.
The target board is a EVMK2H, with the boot mode set to "SLEEP W/ SLOW PLL & SLOW ARM PLL" and the xtcievmk2x_arm.gel GEL script used on the Cortex-A15. This means on a board reset uboot in flash isn't executed, and the GEL script is used to initialize the device.
On starting debug sessions, sometimes the program failed to reach main. E.g. the following sequence is repeatable:
1) Execute a reboot command in EVMK2H BMC to perform a full reset (without having to power-cycle).
2) Start a debug session, and the program doesn't reach main. When suspend the program a Undefined Instruction Exception has occurred on the Cortex-A15.
3) Terminate the failed debug session, and start a new debug session. This time the program reaches main.
By using the ARM Advanced Features to enable "Break on Undefined Instruction" and enable PC trace the undefined instruction is occurring on the FMXR FPEXC,r0 instruction on the following code in the startup_ARMCA15.S file:
.if __ARM_PCS_VFP == 1
@
@ Enable NEON extensions and the VFP. Must be done before entering user mode.
@
MRC p15, #0, r3, c1, c0, #2 @ Read CPACR
ORR r3, r3, #0x00F00000 @ Enable access to CP10 and CP11
MCR p15, #0, r3, c1, c0, #2 @ Write CPACR
MOV r3, #0
MOV r0,#0x40000000
FMXR FPEXC,r0 @ Set FPEXC bit 30 to enable VFP
MCR p15, #0, r3, c7, c5, #4 @ flush prefetch buffer because of FMXR above
.endif
The Enabling Advanced SIMD and VFP extensions section of the ARM Cortex-A15 MPCore Processor Technical Reference Manual shows an ISB instruction after enabling access to CP10 and CP11, which "ensures that all of the CP15 register changes from the previous steps have been committed".
After modifying the startup_ARMCA15.S file to add an ISB instruction after the write to CPACR the program now reaches main() on the first debug session following a full reset:
.if __ARM_PCS_VFP == 1
@
@ Enable NEON extensions and the VFP. Must be done before entering user mode.
@
MRC p15, #0, r3, c1, c0, #2 @ Read CPACR
ORR r3, r3, #0x00F00000 @ Enable access to CP10 and CP11
MCR p15, #0, r3, c1, c0, #2 @ Write CPACR
ISB @ Ensure that all of the CP15 register changes from the previous steps have been committed.
MOV r3, #0
MOV r0,#0x40000000
FMXR FPEXC,r0 @ Set FPEXC bit 30 to enable VFP
MCR p15, #0, r3, c7, c5, #4 @ flush prefetch buffer because of FMXR above
.endif
Suggest the default startup_ARMCA15.S in CCS is modified accordingly.
Also, it looks like the startup_ARMCA8.S and startup_ARMCA9.S have the same problem, although I haven't tested them to see if an Undefined Instruction Exception can occur.