Other Parts Discussed in Thread: SEGGER, , CC3200
Hello,
From the schematic below for AM572x General Purpose EVM Processor Module, it says "Insert wire here to enable use of JTAG without boot image present" on J5. The later part of the sentence is not clear. Does this sentence mean that I have to remove the boot image (say SD card) when trying to short J5 (1 and 2)? OR does it mean JTAG debugging without boot image is enabled when I short J5 (i.e debugging from the host only)?
Another question:
Where do I find information about what to short and how to put the devices in JTAG chain. The above information is from the schematic, but I am looking for some sort of a user manual with same information. Unfortunately, this like does not have that kind of hardware configuration information. http://processors.wiki.ti.com/index.php/AM572x_GP_EVM_Hardware_Setup
I am interested in finding out the position of the devices in the JTAG chain? Are they in a JTAG chain at all? or how to debug if I have connected properly or not etc..
Thank you very much for your time.