Tool/software: Code Composer Studio
I have updated the spectrum emulator driver when installing the CCS 6.2.
When I debug the program the error message show like this :
Description Resource Path Location Type
File connections/SD510USB_Connection.xml does not exist. Was included by file C:/Users/Admin/workspace_v6_2/Example_2834xEPwm_ControlBoard_Test/XDS510USB.ccxml XDS510USB.ccxml /Example_2834xEPwm_ControlBoard_Test line 0 Problem
From previous thread, I already tried the following steps
1. check the SD510USB_Connection.xml file in C:\ti\ccsv6\ccs_base\common\targetdb\connections
2. select the connection as : Spectrum Digital XDS510USB Emulator
3. Verify the emulator connection the message shows connection is good like this:
** Resetting Emulator
-- Emulator is Reset
** Emulator Scan Test
-- Found JTAG IR Length of 38
-- Found 1 device(s) in the scan chain
[End]
4. In the project, I include XDS510USB.xml which has the code like this:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Spectrum Digital XDS510USB Emulator_0">
<instance XML_version="1.2" desc="Spectrum Digital XDS510USB Emulator_0" href="connections/SD510USB_Connection.xml" id="Spectrum Digital XDS510USB Emulator_0" xml="SD510USB_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Spectrum Digital XDS510USB Emulator_0">
<instance XML_version="1.2" href="drivers/sdgo28xusb.xml" id="drivers" xml="sdgo28xusb.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320C28343_0" href="devices/c28343.xml" id="TMS320C28343_0" xml="c28343.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>
Thanks and Regards,
Ben