Other Parts Discussed in Thread: TMDSEVM5517
Tool/software: Code Composer Studio
Team,
We need you urgent help as we have been struggling since last two days to have TIDEP-0077 hardware up and running. Somehow we are able to build the complete project and generate the BF_rt_bios.out file. We are now stuck at porting the BF_rt_bios.out file to C5517 EVM hardware. According to Section-4.1 of TIDEP-0077 design guide once the build is complete, step-8 ask to launch the C5517 target configuration. This step requires .ccxml file to launch target configuration which is missing in the project. However, we generated new .ccxml file using the wizard by selecting XDS510 on-board emulation tool and EVM5517. But still no success.
Another observation is DS1 LED comes-up at the time when USB cable is plugged into J3 connector (EMU USB) and then goes off permanently within 2-3 seconds. The error message we got when trying to test the connection with on-board emulator is "Error -- XDS5510-USB Emulator not connected/enumerated".
I have also attached the photos of the board for you to check the jumper and switch settings. We have already tried different combination.
If you are aware of this problem and have a ready solution please do write us back. Otherwise, we can also have a quick call today or tomorrow to discuss the issue.
Thanks in advance!
Best Regards,
Sharad