This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6748: xds110 dont connect to CCS suddenly

Part Number: TMS320C6748


Tool/software: Code Composer Studio

Hello,

          I am using Code composer studio v7 with XDS110 debug probe. Probe was connecting and working fairly for almost 1 month. Even today 5 minutes before it worked. Today when I tried to launch program I got the error 

Error connecting to the target:
(Error -261 @ 0x0)
Invalid response was received from the XDS110.
(Emulation package 6.0.628.3)

And the debug emulator dont connect. How can I solve this?

Thanks in advance

Shalini

  • Shalini,

    The first point to try and debug this is to see if the Operating System recognized it. If you are using Windows, can you see if the XDS110 entry is shown in its Control Panel? If you are using Linux, can you see if two /dev/ttyACM* devices are present?

    user@host:~$ls /dev/ttyACM*
    /dev/ttyACM0 /dev/ttyACM1

    If these show up, issue the command shown in step 2 of this reference to check if the XDS110 is in the runtime mode and not in DFU mode (this last mode is used to upgrade its internal firmware). If this device is in DFU mode, try to disconnect and reconnect the probe (or connect to a different USB port) and see if it comes back in Runtime mode. 

    In case this stays in DFU mode, then perform all the steps of the reference above to try and re-program your debug probe.

    Other communication issues can be caused by ground loops between the host computer and the target board, which could have caused stress on the XDS110 circuitry. I suggest measuring voltage differences between the board and the PC with a voltmeter and see if you have the presence of any type of ghost voltage or loop.

    Hope this helps,

    Rafael

  • Thank you for reply..Issue resolved when I restarted my PC