This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: XDS100 V2 Does Not Show Up in COM Ports

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

Hello, 

I am using a XDS100 V2 debug probe. From the documentation, I should expect to see two channels under COM Ports in Device Manager. However, I only see the following: 

Is this the intended behavior? It passes the verify connection test and I can debug it but it doesn't work with GUI composer (I can't debug and run GUI composer at the same time). 

Later on, I would like to log data over UART so getting a serial port is important. 

Thanks, 

Graham