Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
After upgrading to ccs8 and simplelink 2.00 my custom board is not more detected, the error that I get is Unknown device. I use MSP FET.
This is the entire error:
CORTEX_M4_0: Trouble Reading Memory Block at 0x20100c on Page 0 of Length 0x4: Could not read device memory CORTEX_M4_0: GEL: Error while executing OnTargetConnect(): Target failed to read 0x0020100C at gGEL_DeviceID=*((unsigned int *) 0x0020100C) [msp432p401r.gel:247] at OnTargetConnect() CORTEX_M4_0: Failed Soft Reset: Could not reset device CORTEX_M4_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x6c88: Could not erase device memory CORTEX_M4_0: File Loader: Verification failed: Target failed to write 0x00000000 CORTEX_M4_0: GEL: File: /Users/miha/workspace_200/hello_MSP_EXP432P401R_tirtos_ccs/Debug/hello_MSP_EXP432P401R_tirtos_ccs.out: Load failed.
Can somebody help me?
Until now everything was working fine but now I've locked the second custom board.
Is this a known issue? How to solve?
Thank you
Miha