Part Number: MSP430F5529
Tool/software: Code Composer Studio
Hi
I would like to know how to use the Line Graph in TI GUI Composer? Because the accepted vaules reading from GUI like these:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5529
Tool/software: Code Composer Studio
Hi
I would like to know how to use the Line Graph in TI GUI Composer? Because the accepted vaules reading from GUI like these:
Hi AartiG,
Yes, I am using online GUI Composer v2 via JSON. I still stuck with the plotting the line graph. I have read two sources, but the question didn't figure out.Here my example code is
var result[];
gc.databind.registry.bind('widget.ti_widget_linegraph.series_0_values', "widget.ti_widget_numberbox.value",
function(result) {
var points_string = "";
for(var i=1; i<result.length; i++){
points_string = result + ";"+ points_string ;
}
return points_string;
});
Would you give me a good example to work properly?Many thanks.
Hi Lynn,
I am not sure if two fields in your json are intended to represent x/y axis in your graph or two different lines. However, if you want to graph two independent lines, then I would suggest that you use Scalar Graph widget. In the binding you would set value_0 property to "v", take a look at tutorial available at link below. The tutorial shows a simple JSON object with a single field, which is bound to a LED widget. The process to bind a scalar graph widgets value_0 property would be the same.
You can configure how big the buffer should be in property page as well.
If you are looking for x/y type graph and V/C fields are corresponding to x/y coordinates, then I would suggest that you create a new customCodec_0.js file (from File->New menu) and take a look at its decode function. There is a commented out example code that shows how to parse json objects. You could insert your data accumulation function there and then add a plotly graph and then configure its x/y properties to graph it. You could probably take a look at application available on second link below (which you can import into GUI Composer designer and expand the folder view to see its files) as an example. The application is implemented not to accept JSON but rather a custom set of data that looks like below, which are readings from two sensors that this particular app uses.
a
1234
b
4567
a
8976
b
3322