Other Parts Discussed in Thread: TMS320DM6446, CCSTUDIO
Hello,
I am getting Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4 following error message when I try to connect
TMS320DM6446 on Code Composer 4.1.3.
It works fine on CCStudio 3.2.
I am using Spectrum Digital 510USB.
=========== Error ====================
Error connecting to the target:
Error 0x80000260/-1137
Fatal Error during: Execution, Initialization, OCS,
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings. If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration.
If this is a multi-core system, the master CPU may not be
releasing the DSP/MCU from reset. Please check your
configuration in CC_setup and/or your GEL file to ensure that
nothing is blocking the DSP/MCU from being released from reset.
========================================
Any help is appreciated!
Sid