Part Number: TMS320C5535
Tool/software: Code Composer Studio
Hello (Ki),
I've put the 'c5535 project I've been working on here:

In case that URL doesn't show up correctly: (look in tags please)
The workspace you want to point to is /tmp1/c55x-sim2 in that repository once you download it.
It's running but the Timer0 IRQ isn't firing. Can you please tell me how to do that? I've tried various dat files with Pin Connect but that doesn't seem to work and/or I'm doing something wrong.
I think this is the latest tool set these simulators ran under - I'm going to try and make a target configuration file for some of the later CCS releases and see if that works - but that won't answer the Timer0
question. I've found some older config files for the simulator (.cfg) - but I don't see any explicit sections or modules for the Timer0/1 peripherals that the docs claim is supported. I tried the pin connect to SINT4 but of course all that did was stall the simulator and I had to kill in task manager.
Any help here appreciated.
Thanks!
John