Hi,
the newest version of UNIFLASH does not work on MAC.
After installation of version 4.5 no connection is possible to the CC3220SF launchpad.
after reinstall of version 4.4 I have the following effect:
1.) Shut off MAC (restart is not enough)
2.) Switch on the MAC
3.) start version 4.4
4.) connect to cc3220sf launchpad (device can connect)
5.) disconnect + remove USB cable
6.) reconnect USB cable + reconnect
7.) no reconnect is possible only shut off the MAC will ever reconnect to the device
BR