Tool/software: Code Composer Studio
Hi,
is is possible to test connection to the controller using CAN?
When I do it now I get following message using CCS 5.5.0:
-----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusb.dll'. An error occurred while soft opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-151' (0xffffff69). The title is 'SC_ERR_FTDI_OPEN'. The explanation is: One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. [End]
Can I somehow change serial to CAN and check (i.e. 'ping') control card? I want to check that there is no problem in connection. I already have CAN transitive and CAN to USB adapter. Can signals somehow be traced from PC to Experimental Kit? Unfortunately I am not able to load so I cannot do the other way around (i.e. tracing from Kit to PC).
If I try to 'Build Project' CAN_TXLOOP_A using CCS 6.2.0 I get Errors and Warning, e.g.:
subdir_rules.mk:21: recipe for target 'DSP2833x_DefaultIsr.obj' failed process_begin: CreateProcess(C:\Users\Igor\AppData\Local\Temp\make7828-3.bat, C:\Users\Igor\AppData\Local\Temp\make7828-3.bat, ...) failed. make (e=5): Access is denied.
Maybe if I load CAN_TXLOOP_A using serial connection and then start CAN transmit and trace signal?!
I apologise for multiple questions in the same post, but trying to explore all options.
Regards