This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: Where to download the GBK language packet for CCS v5.4

Genius 13655 points

Part Number: TMS320C6678

Tool/software: Code Composer Studio

Hello Champs,

Where to download the GBK language packet for CCS v5.4?

Thanks.

Rgds
Shine

  • Shine,

    CCSv5.4 is pretty old.  It is based on Eclipse Indigo.

    The Eclipse language packs for that version are available here:

    Note that these language packs just cover core Eclipse capabilities and not the TI specific features.

    Here is some older information that I was able to find:

    To install a language pack unzip it into your \eclipse folder with in the CCS directory structure. To start CCS in a specific language Eclipse will try to determine what language your Windows is running in and then automatically use the language pack. You can force it to use a specific language by changing your desktop shortcut to use the -nl option.

    Examples:

    Japanese "eclipse.exe -nl ja"

    Chinese "eclipse.exe -nl zh"

    Korean "eclipse.exe -nl ko"

    German "eclipse.exe -nl de"

    Regards,

    John