Tool/software: TI C/C++ Compiler
Dear All,
first to my used environment. It ist CCS 8.1.0.11 and CGT 8.2.4. Parallel build is enabled. A lot files of my project are linked resources.
I post this in the CCS forum because I think the issue is releated to the way how CCS is invoking CGT.
I have run into strange assembler errors during compilation.
It appears that when i have different files with the same filename but in anohter folder hierachy, then the code generation toosl are working on the same assembler file!
If i manually build the files one after another then there is no error. But I see that the same asm file is touched and shows (of course) different content.
Is this behavour known or is there a hack for example with the --asm_directory option to overcome this?
Disabling parallel build is not really an option since i already have an long project build time (~20 minutes after clean)
Looking forward to get some ideas
Bernhard