This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: cl6x compiler exits with segmentation fault when compiling the target code produced with openmp



Tool/software: TI C/C++ Compiler

Hello,

I compiled an applicaton with openmp and forgot to declare a global variable for the target section.

Then gcc and clacc produce the target code which is then compiled with cl6x. With my code cl6x crashes

because of a global varable not declared in the omp target section.

Since my code is very large, I wrote a little c-File, that causes the same problems with the cl6x compiler.

The original error message is:

INTERNAL ERROR: /home/mv/ti-processor-sdk-linux-rt-am57xx-evm-03.03.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/acpia6x experienced a segmentation fault

while processing function (unknown or file scope) file (unknown) line 0

This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.

Then I took the preprocessed c-code and deleted code element by element and at the end I got the following code, which can be used 

to reproduce the error, when compiled with the command at the end (I used the cl6x that was included in the linux sdk 05.01.00.11):

extern int glob;


#pragma omp declare target

void hello()
{

int loc= glob;

}

#pragma omp end declare target

/*

copile with

#!/bin/bash
${HOME}/ti-processor-sdk-linux-rt-am57xx-evm-05.01.00.11/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/cl6x --openmp:device -ppa -mv6600 <NameOfThisFile>
*/

I hope that you can fix this bug and make cl6x print a useful error message.

Regards,

     Stephan

  • Thank you for notifying us of this problem, and for submitting a concise test case.  I am able to reproduce the same behavior.  I filed the entry CODEGEN-5903 in the SDOWP system to have this investigated.  You are welcome to follow it with the SDOWP link below in my signature.

    Thanks and regards,

    -George