Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: UNIFLASH, CCSTUDIO
Tool/software: Code Composer Studio
Dear team,
I am trying to Configure Lanchpad F28069M using CCS v6.2.0, but the devise is not listed in the drop down. Kindly let me know how to proceed. On checking the connection using 'Test Connection' the following error occurs:
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Divya\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
An already open status was returned while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-110' (0xffffff92).
The title is 'SC_ERR_OCS_ALREADY_OPEN'.
The explanation is:
This utility opened the controller but found it already in use.
You must exit other debuggers and utilities that access the
controller because this utility must be the only client.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]
Thanks,
Urvi