This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/TMS320C5515: RTOS/TMS320C5515: CPU load graph show nothing

Prodigy 160 points

Replies: 32

Views: 1679

Part Number: TMS320C5515

Tool/software: Code Composer Studio

CPU load cannot show any data

The following is the version of the tools and software:

CCS version: 5.5.0.00077 

C5500 Compiler Tools version: 4.4.1

DSP/BIOS version: 5.42.1.09

SYS/BIOS version: 6.35.4.50

The emulator that I used is Texas Instruments XDS100v2 

Can anyone give step by step guideline to setup the configuration or installation of required software?

  • Guru 144510 points
    Hi,

    It seems you already have all the software you need, which is already shipped with CCSv5.

    Are you looking for something else for the C55x family of devices? Are you running one of the example projects mentioned by Todd in the original thread to see if the Debug environment is properly working?

    Regards,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    Hi,

    I do not know the exact way to setup the configurations in order to show CPU load.

    The method I used is in CCS Debug, Tools > RTOS Analyzer >  RTA (Legacy) > CPU Load

    I follow some of the thread saying that SYS/BIOS is not supporting C55x family so I doubt this is the main reason why CPU load show nothing.

  • Guru 144510 points

    In reply to Qian Gui Loh:

    Hi,

    The menu option you are selecting is correct. CCSv5.5 fully supports the real-time analysis tools and the C55x family of devices.

    In this case, I strongly suggest you to read the DSP/BIOS User's Guide for details about the CPU Load graph and how to invoke it.
    www.ti.com/.../spru423i.pdf

    And you are right; the SYS/BIOS does not support the C55x family of devices.

    Hope this helps,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    BuildOutput.txt

    Hi,

    I still facing problem as the attached file is my full clean and build result.

    Regards,

    Qian Gui

  • In reply to Qian Gui Loh:

    Hi,

    The previous error have solved but now another issue at Debug mode.

    It shows error:

    No source available for "c_int00() at C:/Users\XWRN37\Desktop\MIPStest\bl_renoir\RPD\atlantis\digital\code\Debug\Renoir_C55_D00.01.02.out:{3} 0xef7c{4}"

    I have no idea how to solve this issue and it block me entering debug mode, if I reset, it could not show c_int00() and still nothing show at my CPU load.

    Regards,

    Qian Gui

  • Guru 144510 points

    In reply to Qian Gui Loh:

    Qian,

    The message above is not an error but instead a simple announcement. This is described at:
    dev.ti.com/.../

    Hope this helps,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    Hi,

    Thanks for the information. However, I still cannot see any thing appear at CPU load data/graph. Raw Logs are working fine. Is there any special setting needed to be aware of at configuration file (.tcf) ?

    Regards,
    Qian Gui
  • Guru 144510 points

    In reply to Qian Gui Loh:

    Qian,

    I will have to pull an expert on these graphs to comment further, especially if you are seeing the Raw Logs.

    Regards,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    Qian,

    Can you get CPU load graph working with the stairstep example in DSP/BIOS ?

    Todd
  • In reply to ToddMullanix:

    Hi Todd,

    I could not get CPU load graph as well using staircase example but there is raw logs too.

    Regards,

    Qian Gui

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.