Part Number: DRV8301-HC-C2-KIT
Tool/software: Code Composer Studio
We are using the DRV8301-HC-C2 kit for turning BLDC motors. We recently purchased a new f28035 control card and tried to debug a new project. When we did this, we got the following error:
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
This control card is brand new, so I don't see how it could be damaged. I've read on these forums that we need to use "wait in reset " mode or perhaps check the flash content of the card? How exactly do I do these things? I'm not sure where to access "wait in reset" mode or the flash content inside CCS.