Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hello,
I am trying to compile the Tida-010003 end node example in debug-push configuration.
Target is cc1310 launchpad
I am using CCS8.
I have the following SDK installed
simplelink_cc13x0_sdk_2_20_00_38
simplelink_cc13x0_sdk_1_30_00_06
I have the following xdctools installed
xdctools_3_32_02_25_core
xdctools_3_50_05_12_core
xdctools_3_50_07_20_core
xdctools_3_51_01_18_core
When compiling I get
Description Resource Path Location Type
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 608, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 629, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 649, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 661, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 675, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 685, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#20 identifier "macTxPwrVal_t" is undefined .ccsproject /6lowpan_ti_15_4_project line 706, external location: C:\ti\simplelink_cc13x0_sdk_2_20_00_38\examples\rtos\CC1310_LAUNCHXL\ti154stack\common\mac_user_config_cc13x0_rftable.h C/C++ Problem
#28 expression must have a constant value mac_user_config_cc13x0_subg_us_euro.h /6lowpan_ti_15_4_project/Application line 125 C/C++ Problem
#28 expression must have a constant value mac_user_config_cc13x0_subg_us_euro.h /6lowpan_ti_15_4_project/Application line 126 C/C++ Problem
#28 expression must have a constant value mac_user_config_cc13x0_subg_us_euro.h /6lowpan_ti_15_4_project/Application line 127 C/C++ Problem
gmake: *** [C:/Users/siva9/workspace_v8/6lowpan_ti_15_4_project/debug_push/obj/mac_user_config.obj] Error 1 6lowpan_ti_15_4_project C/C++ Problem
gmake: Target 'all' not remade because of errors. 6lowpan_ti_15_4_project C/C++ Problem
Here is the build console output file below.
The build settings are shown below.
Could you please advise what I am doing wrong.
Best Regards,
Robert